1. Home
  2. /
  3. Press Release
  4. /
  5. Heilind Now Stocking Molex...
Molex

Heilind Now Stocking Molex Mini-Fit Sr. Off-the-Shelf Discrete Cable Assemblies

WILMINGTON, Mass. (PRWEB) May 26, 2020 ― Heilind Electronics, a leading global distributor of electronic components and authorized distributor for Molex, has expanded its selection of interconnect solutions with the company’s Mini-Fit Sr. off-the-shelf discrete wire cable assemblies. Featuring up to a 50 A current rating, these assemblies are available in a variety of cable lengths and use a compact connector to support both prototyping and global production.

Molex Mini-Fit Sr. connectors are based on a dual-beam female terminal design consisting of four points of contact to establish superb electrical contact performance and reliability. All the connectors in the Mini-Fit Sr. family feature silver-plated contacts and polarized housing to inhibit mismating of the header/plug and receptacle. To inhibit accidental unmating, the connectors offer a positive locking feature that provides secure retention. Additionally, to reduce the risk of terminal backout, the connectors include a Terminal Position Assurance (TPA) retainer to establish that terminals are fully seated in their housings. The units also feature fully isolated header pins and plug receptacle terminals to protect against potential damage during handling and mating.

Molex Mini-Fit Sr. cable assemblies offer up to 50 A per circuit using 8 AWG wire — resulting in an extremely robust, high-amperage interconnect solution for a variety of industrial, consumer, telecommunications, medical, power supply and automotive applications.

Visit the Molex Mini-Fit Sr. Off-the-Shelf Discrete Cable Assemblies page for more information.

About Heilind
Heilind Electronics, Inc. is one of the world’s leading distributors of connectors, relays, sensors, switches, thermal management and circuit protection products, terminal blocks, wire and cable, wiring accessories and insulation and identification products. Founded in 1974, Heilind has locations throughout the U.S., Canada, Mexico, Brazil, Germany, Singapore, Hong Kong and China.

About Molex
Molex brings together innovation and technology to deliver electronic solutions to customers worldwide. With a presence in more than 40 countries, Molex offers a full suite of solutions and services for many markets, including data communications, consumer electronics, industrial, automotive and medical.

View the original press release

Share this page